norelem uses cookies to optimally design and continually improve the website. By continuing to use this website, you agree to the use of cookies. You can find more information about cookies in our Data protection declaration.okay

"Flying kitchen" university project

go back
  • "Flying kitchen" university project

VERTICAL

"Flying kitchen" university project

Leonie S., Annika K. and Jakob M., students at the Burg Giebichenstein University of Art and Design Halle, built a mobile kitchen as part of a university project. The amazing thing about this kitchen is that it was designed for use in a lift!
The project:

Under the moniker "flying kitchen", the three students from Halle, Germany, developed a mobile kitchen as part of a university project. The students decided to try and revolutionise the world of elevators and design a kitchen for use inside them.

After creating an exact 3D model, the individual construction stages began.

An important requirement for the kitchen in small spaces was a high level of flexibility while also requiring ideal working possibilities. The result was an innovative storage system comprising a roller carriage with wall rails. This can be equipped with DIN-compliant Euroboxes.

An additional challenge in this project was to fasten the walls in the lift, since neither bolts nor adhesive were viable options. This problem was circumvented with a "house of cards" system (walls were inserted into one another).

The lift kitchen is used particularly in the following scenarios: offices, universities, hotels, and also for private use in multi-storey buildings.

norelem in the project:

Description

Steel rubber buffers
Stainless-steel hinges

Order No.

»26106-01001055

»27876-052013131